×

Are you in the United States?

Visit our U.S.A. & International site for relevant pricing, distribution and product availability information.

Go to www.StarTech.com

USB 3.0 to HDMI Video Adapter now Available!

NOVEMBER 16, 2011

If you're looking for an external USB video adapter that's suitable for high definition applications, we've just released a product that is sure to impress you!

Our new USB32HDE USB 3.0 to HDMI Adapter takes advantage of the outstanding data transfer speeds supported by the SuperSpeed USB 3.0 interface, to deliver full HD display resolutions up to 1920x1200 (16 or 32-bit) as well as 2-Channel Stereo (48Khz) audio - a substantial improvement over adapters that rely on a USB 2.0 connection.

Aside from its video performance capability, the adapter can also be used in a more scalable capacity - up to 5 USB32HDE adapters can be connected simultaneously, which presents a very convenient way to beef up a high-performance laptop or desktop computer into a multi-monitor system.

The adapter is backward compatible for use with a USB 2.0 connections, however performance will be limited by the host connection bandwidth.

comments powered by Disqus

View Recent blog articles...

RSS Feed

Interests

Computers, emerging technology, audio/video, engineering, product design, system building

Categories
Monthly Articles